Symbol:
Function: From a commit in the History view, a new branch is created for the affected project and is then available in the Branches view.
Call: Context menu of a commit entry in the History view
The command opens the Create branch from commit dialog for defining the new branch.
Dialog: Create Branch from Commit
Source commit |
|
SHA1 |
SHA1 (unique ID) of the commit |
Message |
Commit message of the commit |
New branch name |
Name under which the new branch should appear in the Branches view |
Force |
The new branch is created even if there is already a branch with the same name and even if there are local uncommitted changes. |
Checkout |
The new branch is checked out in the Branches view after it is created. |